LSM6DS3 linux driver for ODR of 1666 Hz
Hello STM,
looking the the mainline kernel for the IMU line, i see some comments in the code that say the only supported ODRs are that of up to 416 Hz. is it possible to run the sensor in high performance mode with the current linux driver? Is there a patchset that provides support for this or is this something that is unsupported with linux?
https://elixir.bootlin.com/linux/v5.12-rc8/source/drivers/iio/imu/st_lsm6dsx/st_lsm6dsx_core.c#L18
regards,
wes