Skip to main content
Visitor II
February 9, 2019
Question

LSM6DS33 SDO always low

  • February 9, 2019
  • 0 replies
  • 856 views

I am interfacing to an LSM6DS33 with an ST32F407using the SPI bus. The SPI is set up as follows:

           Fully Duplex

           Master

           Eight Bit

           Clock is high when Idle

           Data sampled on second edge

           Baud Rate Prescale = 64

When I read the Gyro’s X, Y and Z registers they are all always zero. When I look at the SPI signals with a logic analyzer the MISO (SDO) line is always zero. Attached it logic analyze capture of the initialization sequence. I have tried changing the data sampling edge, the board rate and a lot of the write and read code.  I tried disconnecting MISO, SDO is still always low.

My code is attached. I have tried several different LSM6DS33 and get the same results.

ST32F407 to LSM6DS33 connections are:

ST32F407                               LSM6DS33

Pin 41, PA5, SCL        -          Pin 2 (SCL)

Pin 42, PA6, MISO      -          Pin 4 (SDO)

Pin 43, PA7, MOSI      -          Pin 3 (SDA)

Pin 20, PF7, CS           -          Pin 5 (CS)

+3.3V                         -          Pin 1 & 16

Gnd                            -          Pin, 8, 9, 10, 11, 15, 12, 13

    This topic has been closed for replies.