Skip to main content
Visitor II
November 25, 2016
Question

LSM6DS33 SPI pin functions

  • November 25, 2016
  • 1 reply
  • 622 views
Posted on November 25, 2016 at 04:59

Hi,

As per the datasheet, the pin &sharp3 of the LSM6DS33 device is used as 

1. I2C serial data (SDA)

2. SPI serial data input (SDI)

3. 3-wire interface serial data output (SDO)

In what SPI mode is it used as an input (SDI) and in what mode is it used as an output (SDO)?

Does the device support both 3 and 4-wire SPI interfaces?

Regards,

Prachi

#lsm6ds33
    This topic has been closed for replies.

    1 reply

    ST Employee
    December 1, 2016
    Posted on December 01, 2016 at 12:09

    Hello,

    The LSM6DS33 device supports both 3-wire and 4-wire SPI interfaces.

    The pin #3 is used:

    - as SDI and SDO together in 3-wire SPI mode

    - as SDI only in 4-wire SPI mode

    Please refer to the ''6.2 SPI bus interface'' section of the datasheet.

    Thank you and best regards,

    Petr