Skip to main content
Visitor II
November 23, 2016
Question

LSM6DS33 supply voltage

  • November 23, 2016
  • 1 reply
  • 537 views
Posted on November 23, 2016 at 11:58

Hi,

The typical supply voltage for the LSM6DS33 is 1.8V and the maximum limit is 3.6V. Is it fine if a supply voltage of 3.3V is continously provided to the device?

Regards,

Prachi 

#lsm6ds33
    This topic has been closed for replies.

    1 reply

    ST Employee
    December 1, 2016
    Posted on December 01, 2016 at 12:14

    Hello,

    Yes, since the LSM6DS33 analog supply voltage range is from 1.71 V to 3.6 V it is more than fine if a 3.3V supply voltage is continuously provided to the device.

    Thank you and best regards,

    Petr