LSM6DSL accelerometer data Ready interrupt issue
hello,
i am using stm32F401Re nucleo with stm mems sensor kit (x-nucleo-iks01a2).
i am using cubeMx with mems library from st.
the issue is if i set the accelerometer output data rate 6660 Hz then i got the data ready inerruot with 3329 Hz, which is the half of the ODR.
so the data ready interrupt should be the same as ODR.
i am toggling the pin inside interrupt. so nothing more in side the interrupt function.
any help would be appreciated. thank you