LSM6DSL Drift Specifications
Hello, ST engineers. I am working with a general purpose IMU for a tilt sensor application. I am observing some drift on the sensor while the device is off. I have heard that all IMU's can drift a bit, but I was under the impression that it would happen over a longer period of time. Do you have any specifications or testing data regarding the drift of this IMU over time?
I am observing an offset drift of up to 3mg on some units just overnight. The readings are taken near 0g, but not exactly due to zero-g offset in device. The sensor is temperature calibrated, and the offset drift is measured near the same room temperature to minimize the effect of temperature related drift.
I would also appreciate anyone else who has input regarding if you think this magnitude of drift is reasonable and expected for this sensor?
Thank you,
Russell