Question
lsm6Dsl FIFO continuous mode interrupt problem.
Posted on May 10, 2018 at 14:49
Hello FRIENDS!
I have problem with chip LSM6DSL using.
My purpose is use this chip in the FIFO continues mode. I would like receive interrupt from INT1 pin when FIFO full and read info from FIFO. I am working from STM32L452 processor. I tried some chips with my dev board and I have only one chip working properly. It's mean I received rizing front interrupt from INT1 pin and I can read dates from FIFO.Another chips not provides INTERRUPT. The contacts from microcontroller to chip was checked.My registers set up is:
data = 0x01; data1 = ReadLsm6ds3Register(WHO_AM_I); if(error_status == 1) { acc_error_flag = 1; return; } HAL_Delay(200); //Write to FIFO_CTRL3 register. GYRO not in FIFO, Gyro -- no decimation Register adress is 0x08 data = 0x01; error_status = WriteLsm6ds3Register(data,FIFO_CTRL3); if(error_status == 1) { acc_error_flag = 1; return; } HAL_Delay(200); ReadRegister = ReadLsm6ds3Register(FIFO_CTRL3); HAL_Delay(200); //////////////////// FIFO CONFIGURATION ////////////////// /* Acc 104 hz */ data = 0x60; // 208Hz 0x 60 value is 416hz 0x50 208Hz 0x40 104Hz BW = 1.5KHz Register adress 0x10 error_status = WriteLsm6ds3Register(data,CTRL1_XL); if(error_status == 1) { acc_error_flag = 1; return; } HAL_Delay(200); ReadRegister = ReadLsm6ds3Register(CTRL1_XL); HAL_Delay(200); /* Set FIFO 3rd and 4th NOT in FIFO Register number 0x09 */ data = 0;//0x01; error_status = WriteLsm6ds3Register(data,FIFO_CTRL4); if(error_status == 1) { acc_error_flag = 1; return; } HAL_Delay(200); /* Set Fifo ODR to 104Hz and Continuous mode . Register number 0x0A */ data =0x36; //FIFO continues mode error_status = WriteLsm6ds3Register(data,FIFO_CTRL5); if(error_status == 1) { acc_error_flag = 1; return; } HAL_Delay(200); ReadRegister = ReadLsm6ds3Register(FIFO_CTRL5); HAL_Delay(200); /* Set FIFO ODR to highest value * if (BSP_GYRO_FIFO_Set_ODR_Value_Ext(LSM6DSL_G_0_handle, LSM6DSL_FIFO_MAX_ODR) == COMPONENT_ERROR) { return COMPONENT_ERROR; }*//* Set FIFO_FULL on INT1 Register number 0x0D*/
data = 0x20; //FIFO full flag on INT1 error_status = WriteLsm6ds3Register(data,INT1_CTRL); if(error_status == 1) { acc_error_flag = 1; return; }HAL_Delay(200);
ReadRegister = ReadLsm6ds3Register(INT1_CTRL); HAL_Delay(200); /* Set When the FIFO is used, the IF_INC and BDU bits of the CTRL3_C register must be equal to 1. Register number 0x12*/ data = 0x44; error_status = WriteLsm6ds3Register(data,CTRL3_C); if(error_status == 1) { acc_error_flag = 1; return; } HAL_Delay(200); ReadRegister = ReadLsm6ds3Register(CTRL3_C); HAL_Delay(200);What I do wrong?
Could send me proper registry init sequence and values?Best regards.♯
#lsm6ds3 #mems #lsm6dsl