Question
LSM6DSL: Interrupts aren't latched when the LIR Bit is set to 1
Hello,
Even though I have set the LIR bit to 1, the interrupts aren't latched. In the picture you can clearly see that the interrupt is reset before reading the route register of interrupt 1. The LIR bit is definitely set to 1. I have checked this with lsm6dsl_int_notification_get. Routed to the interrupt 1 is the fifo treshold only. What could be the problem?

Kind regards
Cyrill