LSM6DSL - Temperature Accuracy
We have several units of LSM6DSL in the field and I was looking that this part has an embedded temperature sensor. I would like to understand better the accuracy of this sensor. The datasheet is not clear, showing only this information.
Can I assume the operational range of this sensor is the same as the device (Top = -40~85ºC)?
The datasheet says OFFSET -15/+15 ºC. Is this the accuracy of this sensor?
Since is 16bits for ADC resolution, the minimal step will be 1/256 ºC. And the range will read 25ºC +/- 127ºC?
The AN5040 shows a table of example values
Considering these values looks like each degree are part of the 8bit register, making 1bit/ºC and with integer values. Can anyone help me understand that?