lsm6dsl to catch peak shock load
Hi.
We are trying to configure lsm6dsl to catch peak shock. The usecase is that the sensor should sleep until shock occurs (say above 1g on any axis), cause interrupt and have the value available in FIFO. We are using the STMems_Standard_C_drivers from ST as base. We are using I2C for the communication.
My configuration:
lsm6dsl_device_id_get(&dev_ctx, &whoamI);
lsm6dsl_reset_set(&dev_ctx, PROPERTY_ENABLE);
do {
lsm6dsl_reset_get(&dev_ctx, &rst);
} while (rst);
/*
* Set Output Data Rate
*/
lsm6dsl_xl_data_rate_set(&dev_ctx, LSM6DSL_XL_ODR_416Hz); //
/*
* Set full scale
*/
lsm6dsl_xl_full_scale_set(&dev_ctx, LSM6DSL_4g);
lsm6dsl_wkup_threshold_set(&dev_ctx, 4);
routing2.int2_wu = 1;
delay_ms(4); /* per ST AN5040*/
lsm6dsl_pin_int2_route_set(&dev_ctx, routing2);
lsm6dsl_fifo_xl_batch_set(&dev_ctx, 1);
lsm6dsl_fifo_data_rate_set(&dev_ctx,LSM6DSL_FIFO_104Hz);
lsm6dsl_fifo_mode_set(&dev_ctx, LSM6DSL_BYPASS_TO_STREAM_MODE);Few registers:
INT2_CTRl: 0
md2: 20
PULSE_CFG_G: 0
TAP_CFG: 80
INT2_CTRl: 0
FIFO_CTRL3: 1
FIFO_CTRL5: 24
master config: 0
ctrl1: 68
ctrl2: 0
ctrl3: 4
ctrl4: 0
ctrl5: 0
ctrl6: 0
ctrl7: 0
ctrl8: 0
ctrl9: e0
ctrl10: 0Problem is that the I would like to get fifo full interrup when the interrupt occurs. I normally get several interrupts per shock. The fifo isn't even nearly full (about 3-17 samples).
I tried then to route the fifo full interrupt to int1 (which I actually listen) and the shock to int2 (which is just trigger to start filling the FIFO)
routing1.int1_full_flag = 1;
lsm6dsl_pin_int1_route_set(&dev_ctx, routing1);However this causes even more interrupts.
***********************************************************
I've been through the application note (AN5040), however it doesn't define usecase for maximum shock detection and especially configuring the fifo to get the value for it.