LSM6DSL - values not correct
Hi :)
i m using LSM6DSL accelometer . i My sensivity is -2g/+2g. I have 16 bit (65535 values ) . Well, when i take values, i have values as:
65,423- 64,912 - 16,076
325 - 61,613 - 58448
I dont undestand this value. I think 16,076 is 1 g. And It's ok. But 65535 is 2 g ?
i m supponing 65 635 is 2 g, 32 500 is 0 g , 0 is -2 g.
It ' s correct ?
My real values are not correct ? or correct ?
How is the progession of values ?