LSM6DSLTR Threshold event
Hi!
I’m using the LSM6DSLTR, and really just need to trigger an interrupt whenever the device rotates at a speed greater or equal to a given threshold.
Do I need to set up any FIFO data, or is there a way to only generate an interrupt based on a rotation threshold?
I’ve set the gyro to a full scale selection of +/- 500 dps assuming this would be the threshold setting? (CTRL2_G register)
Curious if anyone else has used this chip to detect a threshold event in a rotation axis?