Skip to main content
Visitor II
October 18, 2017
Question

LSM6DSM Latency and Detailed Model

  • October 18, 2017
  • 1 reply
  • 654 views
Posted on October 18, 2017 at 13:51

Hello everyone,

I am using LSM6DSM in a optical stabilization system. And I would like to construct detailed sensor model. On the datasheet, there is a diagram which shows gyro output structure roughly. Sensor latency and low pass filter types are not given. Is there anyone who knows the internal pattern of the sensor. For example, resonance frequency, internal clocks/ latency and LPF1 and LPF2 structures.

Best regards,

    This topic has been closed for replies.

    1 reply

    ST Employee
    October 19, 2017
    Posted on October 19, 2017 at 11:00

    Hello,

    unfortunately these information are confidential and cannot be shared on the forum.