Skip to main content
Graduate
July 3, 2020
Solved

lsm6dso and lsm6dsox SW detection

  • July 3, 2020
  • 3 replies
  • 2726 views

We use two types of sensors for our dev: lsm6dso and lsm6dsox. It is necessary to detect the type of sensor SW (without opening the device). And it's difficult, because adress (we use i2c) is the same, Device Identification (Who am I) is the same for LSM6DSO and LSM6DSOX... and i can't imagine how to easy to detect it

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Sorry, I have confused. The progression 0-->4 indicates the part number evolution

    STEVAL-MKI197V1 --> LSM6DSOX --> S4

    STEVAL-MKI196V1 --> LSM6DSO --> S0

    regards

    3 replies

    ST Employee
    July 3, 2020

    Hi @YRakh.1​ , since the sensors are very similar, you could distinguish them from the top marking. Can you please send me an image of them? No to easy to distinguish them via SW, because they differs only from MLC embedded digital feature (and it is not so easy to simply "enable" it...) Regards

    YRakh.1Author
    Graduate
    July 3, 2020

    0693W000001s6i1QAA.jpg0693W000001s6hwQAA.jpgthanks for the quick answer! here are the images:

    ST Employee
    July 3, 2020

    Thank you @YRakh.1​ . Please condider the two-digit marking near the pin1 dot indicator

    • marking S0 --> LSM6DSOX device
    • marking S4 --> LSM6DSO device

    Regards

    YRakh.1Author
    Graduate
    July 3, 2020

    Mmm.. are you sure? i just checked STEVAL-MKI197V1 with LSM6DSOX and on this chip label is S4, but it is 100% LSM6DSOX (if datasheet is ok)

    here S4 label:0693W000001s8RbQAI.jpg

    probably you messed up the labeling?

    YRakh.1Author
    Graduate
    July 3, 2020

    got it! thank you! (but to be honest I'm now not 100% sure)