Skip to main content
Visitor II
April 13, 2021
Question

LSM6DSO FIFO Timestamp Gets Reset After 0xFFFF

  • April 13, 2021
  • 1 reply
  • 591 views

Any ideas on why the timestamp gets reset in FIFO after 0xFFFF? I have TIMESTAMP_EN bit of the

CTRL10_C register set to 1 and the DEC_TS_BATCH_[1:0] bits of the FIFO_CTRL4 are set to 01 (max(BDR_XL[Hz],BDR_GY[Hz]) [Hz]).

    This topic has been closed for replies.

    1 reply

    ST Employee
    April 14, 2021

    Hi @BDiva.1​ ,

    there are two reason for which the timestamp can reset:

    you wrote that it resets after 0xFFFF, but what register are you reading? is it TIMESTAMP 0 and 1, or 2 and 3?

    Niccolò