LSM6DSO FIFO with temperature data
Hi!
I'm making driver for LSM6DSO, and I'm stuck with temperature data in FIFO. I understand logic for calculating temperature sensor ODR, based on acc/gyro ODRs, but there is small problem: there is no option to set 26Hz data rate for temperature (in FIFO_CTRL4 there are only 3 options: 1.6Hz, 12.5Hz, 52Hz). So what can I do, when acc ODR is 26Hz, and AN says: "If the accelerometer is configured in Ultra-Low-Power or Low-Power mode and its ODR is lower than
52 Hz, the temperature data rate is equal to the configured accelerometer ODR;"? (26Hz is valid Low Power mode ODR setting).
Best!
ms