LSM6DSO Int2 on Int1although it is disabled
Hi,
we are using the LSM6DSO in Fifo mode and with the double tap feature. Our firmware configures the Sensor Frontend to give an interrupt at fifo_th on INT1 and for double_tap on INT2. Therefore, we explicitly disabled the INT2_on_INT1 bit inside the CTRL4_C register.
But still we see the the INT2 interrupts on the INT1 line. (See plot)
We always reset the sensor to default. So I guess it seems something is not correctly configured.
Here is the code for configuring the sensor:
// configure for the first time
ret_code_t err;
// Get ID
err = lsm6dso_device_id_get(whoamI);
if (whoamI[0] != LSM6DSO_ID){
APP_ERROR_CHECK(NRF_ERROR_NOT_SUPPORTED);
}
// Do reset
uint8_t res;
err = lsm6dso_reset_set(PROPERTY_ENABLE);
do {
lsm6dso_reset_get(&res);
} while (res);
// Disable INT2_on_INT1 to avoid wrong Interrupts
lsm6dso_ctrl4_c_t ctrl4_c = {0};
ctrl4_c.i2c_disable = PROPERTY_ENABLE;
ctrl4_c.int2_on_int1 = PROPERTY_DISABLE;
writeReg(LSM6DSO_CTRL4_C, (uint8_t *)&ctrl4_c);
// Disable I3C
NRF_LOG_INFO("Disable I3C");
lsm6dso_i3c_disable_set(LSM6DSO_I3C_DISABLE);
nrf_delay_ms(10);
// Set BDU
NRF_LOG_INFO("Set BDU update");
lsm6dso_block_data_update_set(PROPERTY_ENABLE);
nrf_delay_ms(10);
// Set power modes
lsm6dso_gy_power_mode_set(LSM6DSO_GY_HIGH_PERFORMANCE);
lsm6dso_xl_power_mode_set(LSM6DSO_HIGH_PERFORMANCE_MD);
// Set FIFO WATERMARK
NRF_LOG_INFO("Set FIFO Watermark!");
err = lsm6dso_fifo_watermark_set(WATERMARK_LEVEL);
APP_ERROR_CHECK(err);
nrf_delay_ms(10);
NRF_LOG_INFO("Set FiFo Batch");
lsm6dso_fifo_batch_set(LSM6DSO_GY_BATCHED_AT_1667Hz, LSM6DSO_XL_BATCHED_AT_1667Hz);
nrf_delay_ms(10);
// Set fifo mode
NRF_LOG_INFO("Set FiFo Mode");
lsm6dso_fifo_mode_set(LSM6DSO_STREAM_MODE);
lsm6dso_pin_int1_route_t pin1;
pin1.double_tap = PROPERTY_DISABLE;
pin1.single_tap = PROPERTY_DISABLE;
pin1.fifo_th = PROPERTY_ENABLE;
lsm6dso_pin_int1_route_set(pin1);
NRF_LOG_INFO("Setting Interrupt Config");
nrf_delay_ms(10);
NRF_LOG_INFO("Set ODR");
lsm6dso_xl_data_rate_set(LSM6DSO_XL_ODR_1667Hz, LSM6DSO_16g);
nrf_delay_ms(10);
lsm6dso_gy_data_rate_set(LSM6DSO_GY_ODR_1667Hz, LSM6DSO_2000dps);
nrf_delay_ms(10);
// set double tap
lsm6dso_double_tap_set();
lsm6dso_pin_int2_route_t pin2 = {0};
pin2.double_tap = PROPERTY_ENABLE;
pin2.single_tap = PROPERTY_DISABLE;
lsm6dso_pin_int2_route_set(pin2);
NRF_LOG_INFO("Config completed");
Any help or comment would be apreciated.