LSM6DSO just one interrupt at high frequency
Hi,
I am using a LSM6DSO and ESP32 to read it.
I am handling the FIFO FULL interrupt by adding a new task to a queue in order to print a message and in the main loop I am reading the buffer of the sensor.
It is working perfectly at 833Hz, but if I set it to 1667Hz, I get the FIFO FULL interrupt just once and then it stops.
I am thinking that the problem may be from ESP32, but what stops the sensor to give another interrupt once I emptied the FIFO? I am using a logic analyzer and I can see that I have the interrupt, the SPI FIFO reading and no interrupt after that.
Regards,
Gabriel