Question
LSM6DSO Register - WAKE_UP_THS - 0x5B
Hi,
I am looking at the LSM6DSO device, and I am unclear what the "USR_OFF_ON_WU" bit does in the "WAKE_UP_THS " register. Does this bit:
- Drive the Wake-Up function with offset corrected accelerometer data? 0 means not offset corrected, 1 means offset corrected?
- What does this have to do with High-Pass Filtered Data? Does this bit actually set whether Lowpass or Highpass information is used to drive the Wakeup Function?
Can someone please provide clarity?
thanks