LSM6DSO Single + Double tap (LIR bit = 1) => Only single tap interrupt.
According to AN5192 (last paragraph of page 50) if LIR is enabled (0x56:0x4F) and SINGLE_DOUBLE_TAP is set (0x5B:0x80) "latched mode is applied to the double-tap interrupt signal only".
But I only read single tap in TAP_SRC (0x1C:0x20) during ISR.
As soon as I disable LIR I get both interrupts.
Is there an error in AN5192 and only single tap will be signalled when LIR = 1?
Or I made a mistake somewhere in the registers?
Here is my register dump:
# i2cdump -yf 1 0x6a
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 00 00 3f 00 00 00 00 00 00 00 40 00 00 08 00 6c ..?.......@..?.l
10: 60 28 44 08 60 00 00 00 e2 20 02 0f 00 20 07 28 `(D?`...? ??. ?(
20: b3 01 0d 00 ee ff f5 ff b2 01 23 00 63 41 00 00 ???.?.?.??#.cA..
30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
40: cd 05 20 00 f3 05 20 00 00 04 00 00 00 00 00 00 ?? .?? ..?......
50: 00 00 00 00 00 00 4f 06 86 06 8a 80 00 00 4a 00 ......O?????..J.
60: 00 00 00 fd aa 01 00 00 00 1a 21 21 40 06 00 00 ...???...?!!@?..
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................