Skip to main content
Super User
March 1, 2021
Solved

LSM6DSO vs LSM6DSOX

  • March 1, 2021
  • 1 reply
  • 2479 views

Is the only difference between the two that LSM6DSOX has the machine-learning core (MLC)?

In other words, are the 2 parts interchangeable when the MLC is not used?

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Andrew Neil​ ,

    basically yes, if you don't mind the MLC feature the two part numbers are interchangeable.

    -Eleon

    1 reply

    ST Employee
    March 2, 2021

    Hi @Andrew Neil​ ,

    basically yes, if you don't mind the MLC feature the two part numbers are interchangeable.

    -Eleon

    Super User
    March 2, 2021

    Great - thanks.

    So, if you have an existing design with LSM6DSO, you could just drop-in an LSM6DSOX to gain the MLC features?

    In fact, I have an X-NUCLEO-IKS01A3 (with LSM6DSO) - so I could use that to get started, and just add MLC stuff later when/if I move to LSM6DSOX ?

    ST Employee
    March 2, 2021

    Yes, that's right, you can take a STEVAL-MKI197V1 and plug it on the DIL24 connector of the X-NUCLEO-IKS01A3 (without un-soldering previous LSM6DSO).

    -Eleon