LSM6DSO32 calibration
Hello,
I made a special card design that includes LSM6DSO32. I want to use this sensor in motion classification project. I want to ask a question about a subject that is said by everyone but I do not know.
Everyone has mentioned that it is necessary to perform a calibration process to get the correct data from an IMU.
However, the LSM6DSO32 sensor's user manual states that it comes calibrated from the factory. Do I need to calibrate this sensor extra?
If yes, how should I do this for accelometer and gyro?
I read an article about the need to subtract the gyro values from the new gyro values by averaging at the stationary position, is this a correct way to calibrate?
I do not know how to calibrate the accelometer. I need help on how to calibrate both gyro and accelometer values.
Without doing any calibration, I set, the gyro is 1000 dps and accel is 8G and the sampling frequency of both to 104 Hz. The values I measured under these conditions are as in the picture. The IMU sensor's position is constant and perpendicular to the Z axis.
Thank for helping.
King regards,
Buse.