Skip to main content
Visitor II
November 22, 2023
Solved

LSM6DSO32X output data is it right?

  • November 22, 2023
  • 2 replies
  • 1347 views

sygo_0-1700640914852.png

I used the lsm6dso32x_read_data_polling example and got the same result as above.(with SPI)

Is this the correct value?

sygo_1-1700641577725.png

And when I checked the values ​​using Unico GUI tool, I got the same values ​​as above.

Although the values ​​are similar to the example, they are slightly different. So I'm a little confused. Is this okay?

Thank you.

    This topic has been closed for replies.
    Best answer by Federica Bossi

    Hi @sygo ,

    Your data seem ok, I don't know in which position you had the sensor but they make sense.

    The little difference between the two measurements can be due to little movements between the first and the second one.

    2 replies

    Technical Moderator
    November 22, 2023

    Hi @sygo ,

    Your data seem ok, I don't know in which position you had the sensor but they make sense.

    The little difference between the two measurements can be due to little movements between the first and the second one.

    sygoAuthor
    Visitor II
    November 23, 2023

    Hi, Federica Bossi

    Thank you for your answer.

    And I have one more question

    An5629 Datasheet Section 8 FSM Configuration Example implemented only Accelerometer.

    I don't understand.

    It seems that you did not set what data you use with FSM, but I don't understand how it was used as an Accelerometer.

    How can you tell me how to use it as an Accelerometer?

    Also, Can you tell me specifically how to create the Threshold? I don't quite understand.

    Technical Moderator
    November 23, 2023

    Hi @sygo ,

    Can you open a specific topic for this question? so that if other users have the same doubt they can find an answer more easily. I also ask you to select the answer to your previous question as accepted solution. Thank you!
    As soon as you create the new question I will answer it :)