Question
LSM6DSOX Example
Hi, I'm developing a project with a NUCLEO-WB55RG and I need to to communicate with a STEVAL-MKI197V1. I'm using the CUBE IDE v1.13.1 and the X-CUBE-MEMS1 v10.0.0. But I'm having a problem when trying to initiate the library calling LSM6DSOX_Init function the program gives me a Hard Fault. I'm trying to use a SPI to communicate with the module.
Is there any examples I can use as guide?