[LSM6DSOX] Inertia motion unit - Incorrect INT1 default pin state
Hi,
I’m encountering an issue with the LSM6DSOX IMU INT1 pin behavior during initialization. The expected behavior is for INT1 to remain LOW by default, including after a software reset. However, what I’m seeing is:
After power-up or reset, the INT1 pin stays HIGH by default.
It only transitions to the expected state (LOW) after the interrupt is configured and routed to INT1.
- I have checked the INT2, it is OK (default LOW)
This is causing some unintended behavior during system startup, as other components relying on the INT1 state assume an interrupt has already occurred.
Expected behavior:
The INT1 pin should be LOW by default and remain LOW after a software reset, until a valid interrupt condition is met.
Has anyone experienced similar behavior, or is there any recommended workaround or configuration to force INT1 to stay LOW until explicitly triggered?
Appreciate any insights or guidance on this.
Thanks