LSM6DSR is never setting XLDA in status reg.
I am trying to validate a new board layout and am looking for the minimal configuration to read accel data.
I'm using SPI. When the WHO_AM_I register of the LSM6DSR is queried, the correct response of 0x6B is returned.
I take that as validation of the at least the layout and soldering.
Looking at AN5358 "Mode 1 - Reading output data" the minimum configuration is to write 0x60 to CTRL1_XL (0x10U), section 4.1. Enabling an ODR of 416 Hz at +/- 2g.
AN5358 in section 4.2 then indicates read STATUS_REG until the LSB, which is XLDA, is set.
That bit is never getting set. Why? STATUS_REG always reads as zero.