LSM6DSV ActivityDetect with no interrupt or routed to INT2 works, routed to INT1 doesn't
I am enabling the LSM6DSV FSMs, SFLP, and SensorHub (LPS22DF slave) to send data to the FIFO where I read it upon INT1 pulses. I also have the embedded TILT function working routed to INT1. If I try to route the activity/inactivity detect to INT1, I get no interrupt function at all. If I instead choose INT2 for the activity/inactivity INT routing, or specify no interrupt for this function, everything works. That is, I see the FIFO data until the inactivity condition is met, and then the data stops until I move the device, as it should. However, without an interrupt for the activity/inactivity detect I have no indication when the device changes state, which I use to power off other devices in the system.
To repeat, this all works as it should when I have the activity/inactivity detect routed to INT2, but I am using the LPS22DF now as a slave to the LSM6DSV master and the LPS22DF data ready interrupt is on LSM6DSV INT2. This allows the LPS22DF data to get into the LSM6DSV FIFO for FSM processing. I suppose I can also do this by using the internal accel as the slave ODR but is there some reason the activity/inactivity detect function cannot use INT1 along with other functions?