LSM6DSV IMU sensor hub with external 3-axis 18-bit high precision magnetometer sensor
Hello,
We want to use LSM6DSV IMU sensor with external 3-axis 18-bit high-precision magnetometer sensor through IMU sensor hub function also with its FIFO function. We refer to following LSM6DSV sensor hub example:
We found that we can't get 3-axis 18-bit (3 x 3 = 9 bytes) mag sensor data from above example. It seemed that we can only get 3-axis 16-bit (3 x 2 = 6 bytes) through sensor hub with FIFO function. Because our total sensor data size has 9 bytes more than 6 bytes, we don't know how to use sensor hub to get 9 bytes mag sensor data with LSM6DSV. Could you give us some suggestion to acquire 9 bytes data from sensor hub or workaround method?
Thank you very much.
Nan