LSM6DSV16X chip does not work.
LSM6DSV16X chip does not work.
I purchased the LSM6DSV16XTR chip, then looked at the datasheet and built a simple circuit.
But SPI communication doesn't work.
I used the LSM6DSV16X arduino library provided by Sparkfun, but communication was not possible.
What's really strange is that I took the chip from the Sparkfun LSM6DSV16X breakout board and attached it to the circuit I designed, and it worked fine.

When I first start up the sensor, do I need to initialize it in a specific way?
Or maybe the delivery was wrong?
The LSM6DSOX chip also has the same pin layout, and I tried soldering it the same way, but SPI communication does not work.
Is there something I need to set up first? I'm sad because I'm a beginner.