Lsm6dsv320 fsm interrupt issue
I designed a fsm Design for high G application. The odr of high G and fsm are same. The said functionality is generating interrupt when done on eval kit Nucleo board with iks4a1 kit in Mems studio. But when I converted it into header file and loaded in another sensor board with lsm6dsv320. It is not working. Earlier Free fall Fsm was done on same sensor, it worked both in mems and on this sensor board. I have called the fsm load function and enabled the embedded interrupt in MD2_CFG as I am generating interrupt on int 2. Odr and range settings of high G have been done seperately. What can be the reason of non functioning.