Question
LSM6DSV32X Power Modes
Hello,
I am working on migrating from the LSM6DSO32 to the LSM6DSV32X for my application. My primary interest in the newer part is the increased gyro range to 4000dps. I am trying to keep the operation of the device similar to what I am using now.
Some of the operating modes have changed and I have a couple of questions.
- The gyroscope no longer has a "Normal" mode. Is "Low Power" mode the next best option to use? If not, which is?
- The accelerometer no longer has "Ultra Low Power (ULP)" mode. It appears the lowest power option available is LPM1. Is this correct? Also, throughout the datasheet, LPM1 is noted as "2 mean." Can this be explained more? Does this factor into the decision of what data rate I need to select (for example if I was using 12.5 Hz previously, would choosing 15 Hz yield the closest performance or would I have to choose double that to account for some sort of filtering?)