Question
LSM9DS0 debugging
Posted on July 11, 2016 at 22:52
Hi all,
I've recently bought a couple of LSM9DS0's for a simple project. Before soldering them to my board I tried to checked if everything was right. I ONLY connected pin 5 and 6 to GND and 15, 16 and 17 to 3v3. However when I turned on the power supply, it showed up a short circuit. I was wondering if anyone has an idea on what is wrong. I don't think that I burnt them by static as I used them with a wrist band connected to GND. Besides, the cut-off current on the power supply is set to 200mA. I'm also attaching the design of the board I was planning to use with the IMU if anyone has an opinion about it. Best regards