Question
LSM9DS1 acceleration anti-aliasing filter
Posted on June 24, 2016 at 11:23
Hi all,
I have some questions regarding the LSM9DS1: 1. The Acceleration ODR choices go down to 10 Hz, however the bandwidth selection, presumable an anti-aliasing filter, is limited to 50Hz. Thus, when sampling at 10Hz or 50Hz with a bandwidth selection of 50Hz severe aliasing is to be expected. Is there a way to avoid this? 2. The accelerometed digital filter operation is not documented properly. What dow ''high resolution'' refer to? How is LPF or HPF selected? 3. Is there a block diagram for the acceleration signal available, similar to Figure 28 in the datasheet for the gyro signals?