Skip to main content
Visitor II
May 28, 2019
Question

LSM9DS1 Activity/Inactivity function details

  • May 28, 2019
  • 1 reply
  • 617 views

How are the Activity/Inactivity registers used? ACT_THS (04h) and ACT_DUR (05h)

Can the LSM9DS1 be configured to automatically go to low-power mode, or does the host need to do that?

    This topic has been closed for replies.

    1 reply

    ST Employee
    May 30, 2019

    Hi Damon, you can select the operating mode during inactivity in register ACT_THS (04h): if you set the SLEEP_ON_ INACT_EN to 0, gyroscope goes in power-down; while setting the bit to 1, the gyroscope in sleep mode. Regards