LSM9DS1 BDU Details
Hi everyone,
Does the block data update mode block also the sensor's sampling? Or simply the sensor continues to acquire and the registers are just not updated until the next reading? It's very important to me because I use LSM9DS1 gyroscope and accelerometer in free run mode at 119 Hz and I read each sample every 10ms (100Hz), in combination with the magnetometer used in single conversion mode: if the accelerometer and gyroscope continue to sample, magnetometer and gyroscope+accelerometer are not synchronous, or their samples are not equally spaced each time.
I hope I was clear,
Thanks,
Daniele