LSM9DS1 FIFO behavior
Hi,
I'm having some problem using the LSM9DS1 FIFO...
My objective is to continuously acquire, without loosing samples, the Gyro and Accelleration data. (The magnetometer is turned off)
This is what I do:
- I set the watermark threshold to 21 samples (IMU_FIFO_samples = 21
(IMU_FIFO_samples = FlashBuffer_Initialize(IMU_6);)
- I configure the interrupt to be sent to pin INT1_A/G
(LSM9DS1_configInt(XG_INT1, INT_FTH, INT_ACTIVE_HIGH, INT_PUSH_PULL);)
- I configure the FIFO in Bypass Mode (LSM9DS1_setFIFO(FIFO_OFF, IMU_FIFO_samples);)
-
- In order to start the data acquisition I configure the FIFO in Continous Mode (LSM9DS1_setFIFO(FIFO_CONT, IMU_FIFO_samples);)
(I did try to set the IMU_SAMPLE_RATE to 14Hz and 900+Hz but the results are the same)
void IMU_Initialize(void)
{
uint16_t tst;
IMU_FIFO_samples = FlashBuffer_Initialize(IMU_6);
LSM9DS1_LSM9DS1(IMU_MODE_SPI, XGADDR, MADDR);
settings.accel.sampleRate = IMU_SAMPLE_RATE;
settings.gyro.sampleRate = IMU_SAMPLE_RATE;
settings.mag.operatingMode = 0x03; // Disabled
tst = LSM9DS1_begin();
LSM9DS1_enableBLE(true); // Big Little Indian
LSM9DS1_enableBDU(true); // Block Data Update
LSM9DS1_configInt(XG_INT1, INT_FTH, INT_ACTIVE_HIGH, INT_PUSH_PULL);
//LSM9DS1_setFIFO(FIFO_CONT, IMU_FIFO_samples);
LSM9DS1_enableFIFO(true);
__delay_ms(50);
LSM9DS1_setFIFO(FIFO_OFF, IMU_FIFO_samples);
}
uint8_t Acquisition_Start(void)
{ EX_INT2_InterruptFlagClear(); EX_INT2_InterruptEnable(); LSM9DS1_setFIFO(FIFO_CONT, IMU_FIFO_samples); return BT_OK;}When the Interrupt is generated the following ISR is called
void Data_Acquisition_IMU(void)
{
...// Read Data From IMU
//n5 = LSM9DS1_getFIFOSamples();
//n4 = LSM9DS1_getFIFOSamples();
//n3 = LSM9DS1_getFIFOSamples();
n = LSM9DS1_getFIFOSamples();
LSM9DS1_readAccelGyro_nAll(&FlashBufferIMU[ptr], IMU_FIFO_samples);
n1 = LSM9DS1_getFIFOSamples();
if(n1 > 31)
{
LSM9DS1_setFIFO(FIFO_OFF, IMU_FIFO_samples);
n3 = IMU_INT1_AG_GetValue();
n2 = LSM9DS1_getFIFOSamples();
EX_INT2_InterruptFlagClear();
n4 = LSM9DS1_getFIFOSamples();
LSM9DS1_setFIFO(FIFO_CONT, IMU_FIFO_samples);
}
...
}
++++ PROBLEMS ++++
Once in a while (quite often but not always) the block of data read from the FIFO is wrong (See attached picture)
LSM9DS1_readAccelGyro_nAll(&FlashBufferIMU[ptr], IMU_FIFO_samples);
void LSM9DS1_readAccelGyro_nAll(uint8_t *data, uint8_t n)
{
LSM9DS1_xgReadBytes(OUT_X_L_G, data, 12*n);
}
I read 12*21 = 252 bytes blocks from the FIFO and sometime the data look wrong (see attached picture)
The data should be always 0 but for az.
In order to debug the program I have been reading the number of data samples available in the FIFO when the ISR is called.
// Read Data From IMU
//n5 = LSM9DS1_getFIFOSamples(); //n4 = LSM9DS1_getFIFOSamples(); //n3 = LSM9DS1_getFIFOSamples(); n = LSM9DS1_getFIFOSamples();Reading n5, n4, n3 and n I read inconsistent values
uint8_t LSM9DS1_getFIFOSamples(void)
{return (LSM9DS1_xgReadByte(FIFO_SRC) & 0x3F);}Sometime n5 = 0 (even if the ISR should be called when in the FIFO there should be 21 samples) and immediately after I read n4 = 21 (the expected value)
--> WHY I READ n5 = 0 ???
Sometime n5 = 21 but then I get n4 = 0x3F
--> The reported number of samples in the FIFO changes abruptly ???
Sometime n5 = n4 = n3 = n = 21 and I read the FIFO data
LSM9DS1_readAccelGyro_nAll(&FlashBufferIMU[ptr], IMU_FIFO_samples);
Sometime when I read the remaining samples in the FIFO, instead of reading 0, or at most a small number, I get 0x3F
Once I get 0x3F, in order to read meaningful number samples in the FIFO is to reset the FIFO setting the FIFO_OFF and the re-enabling it by setting FIFO_CONT
Any clue on how to fix it?
Thank you
#fifo #lsm9ds1