LSM9DS1 FIFO usage
Hello,
I tried to use FIFO in way to count data ready . My idea to count sample and if it is a 32 sample in FIFO I read all at once. As far I understand, according by datasheet "
Accelerometer and gyroscope multiple reads (burst)" Page 21
Data stores into FIFO in this way
0, OUT_G_X,OUT_G_Y,OUT_G_Z,OUT_XL_X,OUT_XL_Y,OUT_XL_Z
1, OUT_G_X,OUT_G_Y,OUT_G_Z,OUT_XL_X,OUT_XL_Y,OUT_XL_Z
...
31, OUT_G_X,OUT_G_Y,OUT_G_Z,OUT_XL_X,OUT_XL_Y,OUT_XL_Z
That is my setup of sensor
lsm9ds1_fifo_temp_batch_set(IMU_I2C_ADD, 0);
lsm9ds1_fifo_mode_set(IMU_I2C_ADD, LSM9DS1_STREAM_MODE);
lsm9ds1_fifo_stop_on_wtm_set(IMU_I2C_ADD, 28);
pin_cfg.int1_drdy_xl= 0;
pin_cfg.int1_drdy_g = 1;
pin_cfg.int1_boot = 0;
pin_cfg.int1_fth = 0;
pin_cfg.int1_ovr = 0;
pin_cfg.int1_fss5 = 0;
pin_cfg.int1_ig_xl = 0;
pin_cfg.int1_ig_g = 0;
lsm9ds1_fifo_watermark_set(IMU_I2C_ADD, 32);
lsm9ds1_fifo_watermark_get(IMU_I2C_ADD, &value);
lsm9ds1_filter_settling_mask_set(IMU_I2C_ADD, 1);
lsm9ds1_act_mode_set(IMU_I2C_ADD, 0);This part of function:
unit8_t size_of_sample 6;
unit8_t gyro_and_accel = 2;
uint8_t samples_count = 32;
lsm9ds1_fifo_data_level_get(IMU_I2C_ADD, &unread_samples);
PRINTF("FIFO number of samples %d", unread_samples);
lsm9ds1_read_reg(IMU_I2C_ADD, LSM9DS1_OUT_X_L_G, &data[0], gyro_and_accel * size_of_sample * samples_count) );
lsm9ds1_fifo_data_level_get(IMU_I2C_ADD, &unread_samples);
PRINTF("unread_samples %d", unread_samples);
Expected print out :
>> FIFO number of samples 32
>> unread_samples 0
But I got
>> FIFO number of samples 32
>> unread_samples 8
Why it is 8 samples? It should be 0
My I2C works on 400Hz