LSM9DS1 SDO not tri-stated
I need several LSM9DS1 sensors one the same SPI line. However, I noticed that when CS is high, SDO (aka MISO) is not tri-stated but pulled down to GND.
I thought this was due to the default double-interface (SPI/I2C), so I have enabled the I2C_DISABLE bit in REG9, but nothing has changed.
Thus, I need a tri-state buffer on MISO lines of each sensor.
But the answer here seems different: https://community.st.com/s/question/0D50X00009XkXIPSA3/lsm9ds1-on-single-spi-bus-with-other-devices?t=1611822778772
Anyone can shed some light on this?
Thanks!