make pre-calibration time shorter
Hi
I'm using multiple vl6180x devices and want them to work more quick.
However, when the second device starts in pre-calibration time of first device, the range data looks wrong.
When I set the interval more than 4ms between two devices, their range data looks correct.
So, I guess that in the case that two devices work simultaneously in their pre-calibration time, the interference occurs.
Then, I would like to ask whether I make pre-calibration time shorter than 4.3ms or skip pre-calibration phase.
I read the data sheet of vl6180X and found the pre-calibration time is fixed.
However, I want absolutely multiple vl6180x devices to work simultaneously.
Otherwise, I want them to work more quickly (less than 4ms interval).
Is it possible?
Best regards
Ishikawa
#vl6180 #multiple-vl6180x #vl6180x