Skip to main content
Visitor II
March 28, 2018
Question

Maximum cover window for VL53L1X/VL53L0X

  • March 28, 2018
  • 2 replies
  • 874 views
Posted on March 28, 2018 at 16:07

The previous proximity sensor 

VL53L0X has a application note (AN4907: VL53L0X ranging module cover window guidelines) that specifies the cover window thickness limits for different distances that can be measured.

I wonder if there is a similar document for the new VL53L1X, because so far I could not find any. I need to measure at least 1000mm for a cover window that is 

3mm thick.

Is there is a way to measure the 1000mm with the 3mm cover window for the VL53L0X, that would be even better.

#cover-window #vl53l0x #cover-glass #vl53l1x
    This topic has been closed for replies.

    2 replies

    Visitor II
    April 6, 2018
    Posted on April 06, 2018 at 19:59

    I asked the same question and submitted a ticket to support, their response:

    With the minor exception of the exclusion cones being different sizes and the chip dimensions being slightly different, all that data is still correct.

    Hornix also builds a coverglass for the L1X part. (Slightly different size.) 

    Hope this helps!!

    ST Employee
    May 1, 2018
    Posted on May 02, 2018 at 00:21

    The VL53L0X and the VL53L1X work the same way. The L1X - due to a lens - has better light gathering. Gathering more light is going to make it a better candidate for ranging through particularly bad cover glass. And a 3mm glass is almost the definition of bad in this case. If you didn't like the L0X performance, invest the $50 and try the L1X. You might be pleasantly surprised.