Mems configuration on Custom Board
Hello,
after experimenting MEMS sensors with the IKS4A1, I developed a custom board based on STM32F407 CPU with the LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.
The aim is to get board inclination and compass information with the maximum accuracy.
On CUBE-MX I select the LIS2MDLTR on the "Board Part Mag" section, the LSM6DSV16XTR on the "AccGyrQVar" section.
Then I selected the MotionFX, MotionTL, and MotionEC libraries.
Finally I choose "CUSTOM_TiltSensing" on "MEMS1_Application". At this point the yellow warning message imposed me to add the "MOTION_SENSOR" on the "Board Support Custom" section. It is not clear to me the reason of this and what does it means.
In any case after I had configured all the parameters the connection with MEMS Studio produces a "Board not identified" message.
Does it has some sense to define the MEMS1_application on CubeMx with a custom board? Is it possible to use Mems Studio with custom boards?
Thank you for your support.