Skip to main content
Visitor II
December 15, 2025
Question

MEMS Studio: Failed to parse log file on IR Algorithms Tuning

  • December 15, 2025
  • 1 reply
  • 66 views

I'm using a STEVAL-MKI109D with the IR sensor STHS34PF80 and I need to fine tune it to detect objects with low IR emissivity, but everytime I want to load the log file into the IR Algorithm Tuning, the same error appears "Failed to parse log file". I've tried modifiying different things from the log, but everytime, I get the same error. Here is an example of a log file:

# STEVAL-MKI231KA (STHS34PF80)

time[us],t_object[LSB],t_object_comp[LSB],t_ambient[C],t_ambient_shock[LSB],t_ambient[LSB],t_ambient_shock_flag,motion[LSB],presence[LSB],presence_flag,int_1
638,-614,-614,23.470,0,2347,0,0,0,0,0
638,-671,-671,23.540,0,2354,0,0,0,0,0
729188,-641,-641,23.490,5,2349,0,0,0,0,0
1736289,-659,-659,23.440,9,2344,0,15,15,0,0
2742002,-642,-642,23.450,7,2345,0,12,12,0,0
3748506,-626,-626,23.490,2,2349,0,19,19,0,0
4754121,-617,-617,23.510,0,2351,0,30,30,0,0

Any idea on what could be happening?

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    December 24, 2025

    Hi @RVM ,

    We are not able to replicate your issue. Can you please share your specific file?

    Thanks!

    RVMAuthor
    Visitor II
    December 29, 2025

    Hi @Federica Bossi ,

    here is the file.