Skip to main content
Explorer
December 4, 2025
Question

MEMS Studio MLC Debug tab not available (Version 2.2.0)

  • December 4, 2025
  • 1 reply
  • 73 views

I am currently trying to build a motion detector like application using a LSM6DSV80x and it's MLC in combination with MEMS Studio (fw 2.2.0). To do so, I use the standard DataLogExtended firmware on a NUCLEO-F401RE and can successfully log and visualise data in MEMS-Studio. The MLC training can also be done successfully, and I can flash the MLC from MEMS Studio as well as use the Decision Tree Output Viewer.

But then, when I want to tweak the parameters or understand what is going on, I am missing the MLC Debug Tab in MEMS Studio (as referred to in UM3233 (MLC section) completely and cannot test on already recorded data (see picture attached).

So where can I find the Debug MLC Tab in MEMS Studio 2.2.0? If it was removed, which is the last MEMS Studio version that supports it?

(Tested both on Mac and Windows -> same issue)

 

tizdipietro_0-1764837233564.png

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    December 4, 2025

    Hi @tizdipietro ,

    MLC debug is currently available only on ProfiMEMS.