Skip to main content
Graduate
October 16, 2024
Solved

MEMS Studio reports WHO_AM_I issue when using LSM6DSO16IS Sensor Hub

  • October 16, 2024
  • 1 reply
  • 989 views

I am using NUCLEO_F401RE + X-NUCLEO-IKS4A1 with MEMS Studio software. 

X-NUCLEO-IKS4A1 offers multiple various bus configurations, including the sensor hub mode for LSM6DSO16IS.

TorrisYin_0-1729055728000.png

TorrisYin_1-1729055739422.png

However, only in standard I2C mode can we establish the connection in MEMS Studio. If using the sensor hub mode, there will be WHO_AM_I warning and connection cannot be setup.

The issue doesn't appear in Unicleo-GUI since we can disable the sensor affected, but in MEMS Studio, the option cannot be changed.

TorrisYin_2-1729056098005.png

 

 

    This topic has been closed for replies.
    Best answer by Federica Bossi

    Hi @Torris-Yin ,

    Unfortunately, it is not possible to do this in MEMS Studio, which is why the sensor is not recognized.

    1 reply

    Graduate
    October 16, 2024

    WHO_AM_I Warning:

    TorrisYin_0-1729056334010.png

     

    Technical Moderator
    October 23, 2024

    Hi @Torris-Yin ,

    Unfortunately, it is not possible to do this in MEMS Studio, which is why the sensor is not recognized.