MEMS Studio + X-NUCLEO IKS4A1: LSM6DSV WHO_AM_I register does not match
I could successfully operate the X- NUCLEO IKS4A1 in the MEMS Studio with the default sensor selection on the board. However, when I tried to select the LSM6DSV, which is connected on the DIL24 socket of the X-NUCLEO IKS4A1 board, for the accelerometer and gyroscope sensor configuration in MEMS Studio, I get the following error window:
The WHO AM I register value does not match the device selected
I also connect two jumpers between 9-10 for the headers J4 and J5 on the X-NUCLEO IKS4A1 board and removed the two jumpers between 11-12 for the header J4 and J5.
Do you have some recommendation, what I miss here?
Many thanks in advance.
Best regards
Christian