MotionEC_Initialize generates an error when it is called
Hello,
It seems that the library MotionMC_CM7F_wc32_ot_hard.a is missing the called function, here the error :
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: ../Middlewares/ST/STM32_MotionMC_Library/Lib\MotionMC_CM7F_wc32_ot_hard.a(motion_mc.o): in function `MotionMC_Initialize':
motion_mc.c:(.text.MotionMC_Initialize+0xde): undefined reference to `MotionMC_SaveCalInNVM'
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: motion_mc.c:(.text.MotionMC_Initialize+0x1fc): undefined reference to `MotionMC_LoadCalFromNVM'
I'm just doing like the example, I erased and reinstalled MEMS and this library at the previous version but nothing changes, can you help me ?
Here the call :
#define VERSION_STR_LENGTH 35
#define SAMPLE_TIME 20
/* Magnetometer calibration API initialization function */
MotionMC_Initialize(SAMPLE_TIME, 1);