MP34DT05-A PDM: increase SAI clock frequency
Hello everyone,
I have an application that eventually record some audios and is working fine with a pair of MP34DT01. It works over SAI with a clock of 1.024MHz and a decimation factor of 64 (for the PDM2PCM), leading to an audio frequency of 16kHz.
The problem that I have now, is that I'm migrating the MEMS to MP34DT05-A. It seems to actually be working fine so far, but in its datasheets it states a minimum clock frequency of 1.280MHz. Therefore, ideally I should change the frequency of the SAI interface. I've done it and I've also changed the decimation factor to 80, as explained in AN5027 and UM2372. However, with these new configs, I obtained just noise (like a strong beep). I've checked the clock with the osciloscope and it is indeed 1.280MHz.
Is there any other configuration (maybe related to the DMA?) that I'm missing here in order to be able to increase the SAI clock from 1.024MHz to 1.280MHz?
Is it even necessary to do this frequency change? considering that although the datasheets says that, it seems to be working just fine with 1.024MHz.
Thanks!