MP34DT05-A randome noise
Hello ST community,
I am unfortunately facing a problem with the MP34DT05-A MEMS microphone. I am using the DFSDM module to read in the microphone. Unfortunately, it happens again and again that extremely strong noise is added at a random time (see picture: At first, almost no noise can be recognized. Likewise after the first peak, which is a clap in the recording. After that, however, there is suddenly a very strong noise). I cannot clearly reproduce the behavior, as the noise sometimes occurs from the beginning, then after 2 seconds and so on. I have defined the DFSDM module as follows:
System Clock: 80MHz
Channel 2: mode PDM/SPI input from ch2 and internal clock
Output Clock: Divider 40
Channel 2: Type SPI with rising edge, SPI Clock with rising edge, Filter Order FastSinc filter type, Oversampling 1
Filter 0: regular channel selection Channel 2, Continous Mode, Fast Mode Enabled, Dma Mode Enabled, Sinc Order Sinc3 filter type, Fosr 50, Iosr 1
Has anyone had similar experiences?