My STWINKT1 gets locked up
I am testing STWINKT1 board, it always use to work without any issues. Off late I am having issues to download the compiled codes into the unit.
I connected the unit to ST-LINK Utility , it connects but reports Read out protection is activated.
Luckily I have another board, I connect to this board and disconnect. Then I connect the first board, then the Read out error does not appear, Also I go on to download the codes with debug option.
However it only works in the second attempt.
Also next time I try downloading the codes, again it goes into read out protection activated mode.
So every time I try to download the program, I have to go through this messy procedure.
I do not understand why it is doing like this.
Please find attached screen shots.
Regards
Shaun