Skip to main content
Visitor II
January 12, 2023
Solved

Need 8000 degrees-per-second

  • January 12, 2023
  • 1 reply
  • 1713 views

I have successfully designed a product which uses ISM330DHCX. However this unit only allows for a maximum of +/- 4000 dps, and within the application of the product, the gyro can saturate at high speeds.

Are there any plans on releasing a product that can measure +/- 8000 dps? This range would cover what I need.

Thank you.

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Nate​ ,

    a +/- 8000 dps is not in the very near development roadmap... but why do you need such a wide Full Scale?

    -Eleon

    1 reply

    ST Employee
    January 18, 2023

    Hi @Nate​ ,

    a +/- 8000 dps is not in the very near development roadmap... but why do you need such a wide Full Scale?

    -Eleon

    NateAuthor
    Visitor II
    January 18, 2023

    This is for a sports product, where the player can impart 2000 RPM on the ball.

    ST Employee
    January 24, 2023

    Hi @Nate​ ,

    understood, thank you. I'll report this input internally.

    -Eleon